:CHANnel:RTSCope:TRACk
Command Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:TRACk {ON | OFF}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CHANnel{1:8}{A|B|C|D}:RTSCope:TRACk?
Description
Enables or disables the use of shared software clock recovery settings that are applied to all FlexRT channel input waveforms. Shared settings are made in the :TIMebase subsystem using the:TIMebase:SCRecovery SCPI node. For example,:TIMebase:SCRecovery:STATe.
When you disable shared software clock recovery settings with the :CHANnel:RTSCope:TRACk command, use the commands in the following SCPI nodes to configure unique setting for a specific channel waveform:
:CHANnel:RTSCopecommands:CHANnel:SCRecoverycommands
Start with the :CHANnel:SCRecovery:STATe command to turn on or off software clock recovery.
Requires FlexDCA revision A.06.70 and above.
Example Command
:CHANnel2A:RTSCope:TRACk ON