Common Commands
Instrument:
N1000A
DCA-M
N1010A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Common commands are defined by the IEEE 488.2 standard. They control generic device functions that are common to many different types of instruments. Common commands can be received and processed by FlexDCA, whether they are sent as separate program messages or within other program messages. The *STB?, *SRE, *ESR?, and *ESE commands set and query top-level registers in the status reporting system. Lower-level status registers are controlled using commands in the :STATus subsytem.