:DIFF:YOFFset
Command Syntax
:DIFF{1:8}{A|C}:YOFFset <offset>
<offset> is a double.
Where the required specifier {1:8}{A|C} identifies the differential channel by its module slot and channel letter. For example, the differential waveform of channels 1A and 1B would be identified as :DIFF1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:DIFF{1:8}{A|C}:YOFFset?
Description
Sets the voltage that is represented at the center of the display for the selected differential waveform.Offset parameters are vertical scale dependent. Currently, the offset can be expressed in volts only using the :DIFF:UNITs command. Use the :DIFF:YSCale command to change a channel's vertical scale.
In Jitter Mode, channel scale and offset controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Example Command
:DIFF2A:YOFFset 125.3E-4