:DIFF:YSCale
Command Syntax
:DIFF{1:8}{A|C}:YSCale <scale>
<scale> is a double.
Where the required specifier {1:8}{A|C} identifies the differential channel by its module slot and channel letter. For example, the differential waveform of channels 1A and 1B would be identified as :DIFF1A.
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:DIFF{1:8}{A|C}:YSCale?
Description
Sets the vertical scale ( units-per-division) of the selected differential waveform. Use the :DIFF:YOFFset command to change a channel's vertical offset.
In Jitter Mode, channel scale and offset controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Example Command
:DIFF2A:YSCale 2.00E-1