:DISK:JDATabase:RECall:DESTination
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.70 and above, use the :JDMemory:FILE:LOAD command instead.
Command Syntax
:DISK:JDATabase:RECall:DESTination JMEMory1
Query Syntax
:DISK:JDATabase:RECall:DESTination?
Description
Selects the target jitter database location to load a waveform memory file. Since there is only one jitter database location, the only valid argument for this command is JMEMory1. Use the :DISK:JDATabase:RECall command to actually load the file into the jitter database.