:DISK:JDATabase:RECall
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.70 and above, use the :JDMemory:FILE:LOAD command instead.
Command Syntax
:DISK:JDATabase:RECall
Description
Loads a jitter database file into FlexDCA's one available jitter database location. Use the :DISK:JDATabase:FNAMe command to specify the file to load. Since there is only one jitter database location, the :DISK:JDATabase:RECall:DESTination command always points to JMEM1.