:JDMemory:FILE:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Command Syntax
:JDMemory{1}:FILE:LOAD
Where the {1} is the required specifier that indicates that only one jitter data memory is available at this time, :JDMemory1.
Description
Loads the selected jitter data file into jitter memory. Use the :JDMemory:FILE:NAME command to specify the name of the file to load. Use the :JDMemory:DISPLay command to display the jitter-memory waveform.
To load the current jitter database into memory use the :JDMemory:LOAD command.
Requires FlexDCA revision A.05.70 and above.