:DISK:SIMage:GONLy
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.03.00 and above, use the :DISK:SIMage:WINDow command instead.
Command Syntax
:DISK:SIMage:GONLy {ON | OFF | 1 | 0}
Query Syntax
:DISK:SIMage:GONLy?
Query Response
{1 | 0}
Description
Selects to save only the waveform and graticule in screen captures by the :DISK:SIMage:SAVE command. The menu bar, toolbars, tables, and status bar are not included in the image file. In Jitter Mode, the waveform and graticule are saved as if the Graph panel was closed; jitter result graphs are not included. Any dialogs open and positioned over the viewing area are not saved in the file. When printing a hard copy of the waveform, combined this command with the :DISK:SIMage:INVert command (graticule only) to save ink or toner.