:DISK:SIMage:WINDow
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISK:SIMage:WINDow {DISPlay | TIME1 | GDELay{1:4} | MAGNitude{1:4} | PHASe{1:4}}
Query Syntax
:DISK:SIMage:WINDow?
Description
Selects to save the entire display, including items such as menu bar and toolbars when using the :DISK:SIMage:SAVE command. Or, a specific waveform content window: Waveform, Magnitude, Phase, or Delay. If a waveform content window is selected, use :DISK:SIMage:SINClude to select the which content window waveforms to include in the screen capture. In Jitter Mode, the waveform and graticule are saved as if the Graph panel was closed; jitter result graphs are not included. Any dialogs open and positioned over the viewing area are not saved in the file.
| Argument | Displayed Waveform Content Window |
|---|---|
| DISPlay | The entire display including the currently displayed waveform content window. |
| TIMe{1} | Waveform |
| GDELay{1:4} | Delay |
| MAGNitude{1:4} | Magnitude |
| PHASe{1:4} | Phase |
Requires FlexDCA revision A.03.00 and above.