:DISK:WAVeform:RECall
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.70 and above, use the :WMEMory:FILE:LOAD command instead.
Command Syntax
:DISK:WAVeform:RECall
Description
Loads a waveform memory file into one of eight waveform memory locations. Use the :DISK:WAVeform:RECall:DESTination command to select the waveform memory. Use the :DISK:WAVeform:FNAMe command to specify the file to load.
Example Command Sequence
:DISK:WAVeform:FNAMe "DUT_3_waveform.wfmx" :DISK:WAVeform:RECall:DESTination WMEMory2 :DISK:WAVeform:RECall