:WMEMory:FILE:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:FILE:LOAD
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Description
Loads the selected waveform file (.wfmx, .csv, or .txt) into the indicated waveform memory location. Use the :WMEMory:FILE:NAME command to specify the name of the file to load. Use the :WMEMory:DISPLay command to display the waveform memory.
To load a waveform source into memory, for example channel 1A, use the :WMEMory:LOAD command.
Requires FlexDCA revision A.05.70 and above.