:DISK:WAVeform:RECall:DESTination
Command:
Deprecated
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.05.70 and above, use the :WMEMory:FILE:LOAD command instead.
Command Syntax
:DISK:WAVeform:RECall:DESTination {WMEMory1 | WMEMory2 | WMEMory3 | WMEMory4 | WMEMory5 | WMEMory6 | WMEMory7 | WMEMory8}
Query Syntax
:DISK:WAVeform:RECall:DESTination?
Description
Selects one of eight waveform memory locations to load a waveform memory file. Use the :DISK:WAVeform:RECall command to actually load the file into the indicated memory. You can load all three waveform formats into memory: internal, Y-value, and XY-value formatted files.
Example Command Sequence
:DISK:WAVeform:FNAMe "DUT_3_waveform.wfmx" :DISK:WAVeform:RECall:DESTination WMEMory2 :DISK:WAVeform:RECall