:DISPlay:DIALog:BTRansparent
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:BTRansparent {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:BTRansparent?
Query Response
{1 | 0}
Description
Turns the ability to display dialogs with transparent backgrounds on and off. The default setting is OFF. Use the :DISPlay:DIALog:OPACity command to adjust the level of opacity.
dialog transparency requires Windows Vista or Windows 7.