:DISPlay:DIALog:OPACity
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:OPACity <percent>
<percent> is an int.
Query Syntax
:DISPlay:OPACity?
Description
Sets the level of a dialog's background opacity when dialog transparency is turned on. The opacity can be any value between 0% (clear background) and 100% (solid background). The default setting is 100%. Use the :DISPlay:DIALog:BTRansparent command to turn dialog transparency on.
The ability to set the opacity of a dialog requires Windows Vista or Windows 7.