:DISPlay:SPALette:COMPact
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :DISPlay:SPALette:MODE command.
Command Syntax
:DISPlay:SPALette:COMPact {ON | OFF | 1 | 0}
This command supports the DEFault, TOGGle, and VSET? common child commands.
Query Syntax
:DISPlay:SPALette:COMPact?
Query Response
{1 | 0}
Description
Displays the Signals palette in normal size (OFF) or in compact size (ON). The default setting is OFF. To hide or show the Signals palette, use the DISPlay:SPALette command.