:DISPlay:SPALette
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:SPALette {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:SPALette?
Query Response
{1 | 0}
Description
Hides (OFF) or displays (ON) the waveform Signals palette. This is identical to clicking the Signals button that is located in the display's bottom-right corner. The default setting is OFF. To view the palette in compact mode, use the DISPlay:SPALette:MODE child command. To hide or show the Math palette, use the DISPlay:SSPanel command.