:DISPlay:SPALette:MODE
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:SPALette:MODE {FULL | COMPact | MINI}
Query Syntax
:DISPlay:SPALette:MODE?
Description
Sets the display size of the Signals pallete. To hide or show the Signals palette, use the DISPlay:SPALette command.
- FULL
- Displays the signal palette in its normal default mode. This selection provides the greatest amount of information for each signal, but covers more display area that the other two selections.
- COMPact
- To conserve space, displays the signal palette without showing a representation of the waveforms. The vertical scale-per-division and offset setting are displayed.
- MINI
- Maximizes graticule space by reducing the signal palette to its minimal size. Displays on the signal palette only the buttons to turn the waveform on and off.
Requires FlexDCA revision A.01.70 and above.