:DISPlay:GRATicule:CURSor

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:DISPlay:GRATicule:CURSor {PHAVert | PHORz | ZBOX}

Query Syntax

:DISPlay:GRATicule:CURSor?

Description

Selects the behaviour of the waveform pan and zoom mode, also known as mouse control mode buttons. Waveform pan and zoom is accomplished by dragging the waveform using the mouse touch gestures.

If FlexDCA is installed on a PC or N1000A display which has a capacitive touch display, you can select for these features to respond to touch gestures instead of a mouse. Use the :DISPlay:MULTitouch:STATe command.

Command
Argument
Description Equivalent
GUI Button
ZBOX Drag over a waveform to zoom in on a selected area.
— Reverses a previous waveform zoom. Multiple clicks undos a series of previous zoom actions. There is no command available for this function.
PHAVert Drag to move the waveform in both the vertical and horizontal directions.
PHORz Drag to move the waveform in the horizontal direction. Vertical movement is locked.

Requires FlexDCA revision A.05.00 and above.