:DISPlay:GRATicule:GRID:INTensity
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:GRATicule:GRID:INTensity <intensity>
<intensity> is an int.
Query Syntax
:DISPlay:GRATicule:GRID:INTensity?
Description
Sets the brightness of the display graticule. You can adjust the intensity between the values of 0 (no brightness) to 100 (full brightness). The default value is 100. Use the :DISPlay:GRATicule:GRID:STATe command to turn the display of the graticule on and off.