:GRAPh:T:OHMS:X:SCALe
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
Command Syntax
:GRAPh:T:OHMS{1:4}:X:SCALe <scale>
Where the <scale> is a double.
Where the {1:4} specifier identifies one of four waveform content windows.
Query Syntax
:GRAPh:T:OHMS{1:4}:X:SCALe?
Description
Sets the horizontal scale of the specified Time-Ohmswaveform content window in seconds-per-division or meters-per-division, depending on the setting of the :UNITs sibling command. Use the :POSition sibling command to set or query the time or distance at the display's reference position. The reference position is marked with the
symbol at the top of the graticule. Use the :AUToscale parent command to automatically scale both the waveform in both X and Y axis.
TDR/TDT mode's T-parameter responses are the source of Time-Ohms waveforms.
Requires FlexDCA revision A.04.20 and above.