:LTESt:MTESt:FAILures
Command:
Deprecated
Deprecated command. For FlexDCA revision A.03.00 and above, use the :LTESt:MTESt:MRESult:FAILures command instead.
Command Syntax
:LTESt:MTESt:FAILures <failures>
<failures> is an int.
Query Syntax
:LTESt:MTESt:FAILures?
Description
Specifies the number of total mask violations (failures) required to stop a mask limit test. To enable or disable mask limit tests, use the :LTESt:MTESt:STATe command.