:LTESt:MTESt:MRESult:FAILures
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MTESt:MRESult{1:16}:FAILures <failures>
Where {1:16} identifies the specific mask for which to apply the limit test.
Where <failures> is an int.
Query Syntax
:LTESt:MTESt:MRESult{1:16}:FAILures?
Description
Specifies the number of total mask violations (failures) required to stop a mask limit test. To enable or disable mask limit tests, use the :LTESt:MTESt:MRESult:STATe command.
Requires FlexDCA revision A.03.00 and above.
Example Command
:LTESt:MTESt:MRESult2:FAILures 500