:LTESt:MEASure:SSUMmary:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:SSUMmary:STATe {ON | OFF | 1 | 0}
Query Syntax
:LTESt:MEASure:SSUMmary:STATe?
Query Response
{1 | 0}
Description
Turns on or off the reporting action to save an ASCII summary file whenever a measurement limit test reaches its limit and stops. The file name extension of summary files is .sum. Use the :LTESt:MEASure:SSUMary:FNAMe command to specify the name of the summanry file. The following is an example of a summary file's contents:
Measurement Limit Test Summary 10/07/2011 10:42:44 Mask Region 1 Fails when outside range [0, 0.225] Number of Failures 6 Number of Trials 6 Pass Percentage 0 Mask + Margin Region 1 Fails when outside range [0, 0.225] Number of Failures 6 Number of Trials 6 Pass Percentage 0 Total Mask Hits Fails when outside range [-10, 10] Number of Failures 0 Number of Trials 6 Pass Percentage 100 Total Margin Hits Fails when outside range [-10, 10] Number of Failures 0 Number of Trials 6 Pass Percentage 100 Waveform Count Fails when outside range [-10, 10] Number of Failures 6 Number of Trials 6 Pass Percentage 0 Margin Fails when outside range [-10, 10] Number of Failures 0 Number of Trials 6 Pass Percentage 100