:LTESt:MTESt:SSUMmary:STATe
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MTESt:SSUMmary:STATe {ON | OFF | 1 | 0}
Query Syntax
:LTESt:MTESt:SSUMmary:STATe?
Query Response
{1 | 0}
Description
Turns on or off the reporting action to save an ASCII summary file whenever a mask limit test reaches its limit and stops. The file name extension of summary files is .sum. Use the :LTESt:MTESt:SSUMary:FNAMe command to specify the name of the summanry file. The following is an example of a summary file's contents:
Mask Limit Test Summary 10/07/2011 08:28:25 Total Waveforms, 1 Total Samples, 1533 Mask Margin, 5.0 % Failed Samples, 165 Mask Hits, 131 Margin Hits, 165 Region, Mask Hits, Margin Hits 1, 131, 165 2, 0, 0 3, 0, 0
Example
:LTESt:MTESt:SSUMmary:STATe ON