:LTESt:MEASure:MTESt:LOCation:ULIMit
Removed command for revision A.03.00 and above. This command is no longer available. Use :LTESt:MEASure:MLIMit:ULIMit
insead.
Command Syntax
:LTESt:MEASure:MTESt:LOCation{1:32}:ULIMit <limit>
<limit> is a double.
Query Syntax
:LTESt:MEASure:MTESt:LOCation{1:32}:ULIMit?
Description
Defines the upper limit for a mask measurement limit test in Eye/Mask mode. For example, if you need no more than 10 hits in mask region 1, set the lower limit to 0 and the upper limit to 9 and set the limit test to fail when the hit count is outside the specified limit.
The mask measurement is identified by a number, from 1 to 32, that is appended to the :LOCation
portion of the command. Refer to the :MEASure:MTESt:LOCation:STATe command to learn how to identify the measurement and to turn the measurement limit test on or off. Use the following sibling commands to configure the measurement: