:LTESt:MEASure:MLIMit:ULIMit
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:LTESt:MEASure:MLIMit{1:16}:ULIMit <limit>
Where {1:16} identifies one of sixteen limit tests.
Query Syntax
:LTESt:MEASure:MLIMit:ULIMit?
Description
Defines the upper limit for a measurement limit test. For example, if you chose to measure Oscilloscope Mode's peak-to-peak amplitude and want the upper limit to be 100 mV, you could set the lower limit to 0.1 and then set the limit test to fail when the signal is outside the specified limit. Use the :STATe sibling command to start the limit test.
Requires FlexDCA revision A.03.00 and above.