:LTESt:MEASure:OSCilloscope:LOCation:UPACtion
Removed command for revision A.03.00 and above. This command is no longer available. Use :LTESt:MEASure:MLIMit:UPACtion
insead.
Command Syntax
:LTESt:MEASure:OSCilloscope:LOCation{1:32}:UPACtion {FAIL | PASS | IGNore}
Query Syntax
:LTESt:MEASure:OSCilloscope:LOCation{1:32}:UPACtion?
Description
Selects an action to be taken if the oscilloscope measurement limit test in Eye/Mask mode cannot be performed. The oscilloscope measurement is identified by a number, from 1 to 32, that is appended to the :LOCation
portion of the command. Refer to the :MEASure:OSCilloscope:LOCation:STATe command to learn how to identify the measurement and to turn the measurement limit test on or off.
- FAIL
- If the measurement cannot be made, for example when an edge is expected to be present and is not found, the total number of waveforms is incremented and the total number of failures is incremented. This is the mode to use for most applications.
- PASS
- If the measurement cannot be performed, pass the measurement and do not count it as a failure. You might use
PASS
when triggering on one event and measuring another event which may not occur for every trigger. For example, in a communications test system, you might want to trigger on the clock and test the risetime of edges in the data stream. However, there may be no way to guarantee that a rising edge will be present to measure in the data stream at every clock edge. By using thePASS
parameter, the limit test will not log a failure if there is no edge found in the data stream. If the measurement cannot be made, the total number of waveforms measured is incremented, but the total number of failures is not. - IGNore
- If the measurement cannot be performed, ignore the measurement and do not count it as a pass or fail.
IGNore
is similar toPASS
, except the totals for the number of waveforms and failures are not incremented. Therefore, the total indicates the number of tests when the measurement was made.
Use the following sibling commands to configure the measurement: