Limit Line Commands
Instrument:
N1010A
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Creating an Limit-Line Limit Test
The following example shows how to create an limit-line limit test that runs until a failed data point occures. Notice that the limit line test is first created using :LLINe subsystem commands.
:ACQuire:SINGle :LLINe2:LOAD:FNAMe "%USER_DATA_DIR%\Limit Lines\DUT Input.lltx" :LLINe2:Source CHAN5B :LLINe2:DISPlay ON :LTESt:LLINe:SWAVeform:RESet :LTESt:LLINe:SSUMmary:FNAME "%USER_DATA_DIR%\Limit Summaries\LimitLineTest.sum" :LTESt:LLINe:SSUMmary:STATe ON :LTESt:LLINe:SIMage:STATe ON :LTESt:LLINe:SIMage:INVert ON :LTESt:LLINe:SIMage:WINDow TIME1 :LTESt:LLINe:SIMage:FNAMe "%USER_DATA_DIR%\Screen Images\my test.jpg" :LTESt:LLINe:TEST2:MODe SOFailure :LTESt:LLINe:TEST2:STATe ON :ACQuire:RUN *OPC?