:LLINe Subsystem
Instrument:
N1000A
DCA-M
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
TDR
Use the :LLINe subsystem commands to load, display, and horizontally position a Limit-Line Test file in oscilloscope or TDR modes. There are no commands for creating limit lines. Limit lines can be created using FlexDCA's GUI or an ASCII text editor. Limit lines provide pass/fail testing on single-valued waveforms. A data point "passes" if it is inside the displayed limit lines and "fails" is it is beyond the limit lines. Once loaded, you can shift the limit line relative to the waveform along the time scale.
Use the :LTESt subsystem to stop limit testing on the first passed or failed data point and to report the results.
This subsystem requires FlexDCA revision A.04.50 and above.