:MEASure:AMPLitude:HSYMbol:LEVel
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Command Syntax
:MEASure:AMPLitude:HSYMbol:LEVel {LEVel3 | LEVel2 | LEVel1 | LEVel0}
Description
Selects the logic level at which to perform the HSYMbol measurement. For NRZ signals, select either LEVel0 or LEVel1. For PAM4 signals, select either LEVel0, LEVel1, LEVel2, or LEVel3.
NRZ Waveform
PAM4 Waveform
Query Response
{LEVel3 | LEVel2 | LEVel1 | LEVel0}
Requires FlexDCA revision A.05.60 and above.