:MEASure:AMPLitude:ISI:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude

Command Syntax

:AMPLitude:ISI:LEVel.htm {LEVel3 | LEVel2 | LEVel1 | LEVel0}

Description

Selects the logic level at which to perform the ISI measurement. For NRZ signals, select either LEVel0 or LEVel1. For PAM4 signals, select either LEVel0, LEVel1, LEVel2, or LEVel3.

NRZ Waveform

PAM4 Waveform

Query Response

{LEVel3 | LEVel2 | LEVel1 | LEVel0}

Requires FlexDCA revision A.05.60 and above.