:MEASure:AMPLitude:ISIHist:SAMPles?
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Amplitude
Query Syntax
:MEASure:AMPLitude:ISIHist:SAMPles?
Description
Queries the number of histogram samples used to measure ISI. The number of samples returned is affected by the :MEASure:JITTer:DEFine:EDGe command, which selects jitter measurements based on rising edges, fallingedges, or both edges. For data signals, all edges are included by default. For clock signals, only rising edges are used by default.
If the measurement is unsuccessful, 9.91E+37 (NaN) is returned.
Amplitude analysis must be turned on before the first interference measurement can be made. Use the :MEASure:AMPLitude:DEFine:ANALysis command.
Requires FlexDCA revision A.02.50 and above.