:MEASure:EBOundary:LEFT
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:EBOundary:LEFT <percent>
<percent> is a double.
Query Syntax
:MEASure:EBOundary:LEFT?
Description
Sets the percentage of the symbol period (time) for the eye boundary's left side in Eye/Mask Mode. This setting determines what portion of the eye diagram is used to generate histograms for eye diagram amplitude measurements. The default values of 40% (left) and 60% (right) which identifies the central 20% of symbol period. To set the eye boundary's right side, use the :MEASure:{EYE | CGRade}:EBOundary:RIGHt command. This command is equivalent to the settings in the Eye Boundary tab of the Configure Measurements dialog.