Eye Boundary Commands
Meas. mode:
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
For NRZ signals in Eye/Mask Mode, the left and right eye-diagram boundaries are used to define the central percentage of the symbol period (time). The default value is 40% (left) and 60% (right) which identifies the central 20% of symbol period. You can specify default values or enter your own values using the following three commands.