:MEASure:EYE:APOWer:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:APOWer:SOURce CHANnel{N}
{N} identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Query Syntax
:MEASure:EYE:APOWer:SOURce?
Description
Selects the source waveform on which to perform the APOWer measurement.
The average power measurement is only available when using the modules with integrated optical detectors (optical/electrical modules). Average power measurements cannot be made on simulated channels.