:MEASure:EYE:CEQ:LOCation?
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
PAM4
NRZ
Query Syntax
:MEASure:EYE:CEQ:LOCation?
Description
Returns an index for the location of the measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.:MEASure:EYE:CEQ
Requires FlexDCA revision A.06.00 and above.