:MEASure:EYE:DJ
Command Syntax
:MEASure:EYE:DJ
Query Syntax
:MEASure:EYE:DJ?
Description
Performs an Advanced Eye Deterministic Jitter (DJ σ-σ) measurement in Eye/Mask mode. To return the measurement for a specific eye PAM4 eye diagram, use the :MEASURE:EYE:DJ:EYE command. Since the measurement is made on an eye diagram, the pattern itself can be of any type or length, such as PRBS31. (Jitter Mode is limited to making measurements on patterns up to PRBS16.) The random and deterministic components, RJ and DJ, are determined by analyzing the crossing regions of the eye and measuring random jitter using a Q-scale approach. Separation of RJ is made in the presence of all DJ components using this method. Total Jitter (TJ) is measured at the probabilities specified by :MEASure:EYE:TJ:TJBer. To measure RJ, use the :MEASure:EYE:RJ command. To measure TJ, use the :MEASure:EYE:TJ command.
The query form of the command returns the measured DJ. If the measurement is already on, the measurement listing is moved to the top of the displayed results table.
To increase measurement accuracy, use RJ stabilization:
- In Jitter Mode, measure Random Jitter (RJ) on the signal while using a short pattern.
- Switch to Eye/Mask Mode
- Use the
:MEASure:EYE:DJ:RJSTabilizeto turn on RJ stabilization and:MEASure:EYE:DJ:RJSValuecommands to specify the short-pattern RJ result measured in step 1. - Switch to a long pattern.
- Measure DJ, RJ, and TJ.
Requires Option 401, Advanced Eye Analysis Software license.
This Eye mode measurement can be applied to both NRZ and PAM4 waveforms.
Requires FlexDCA revision A.02.50 and above.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:EYE:DJ
flex.write(':MEASure:EYE:DJ:SOURce CHAN1A')
if flex.query(':MEASure:EYE:DJ:STATus?') == 'CORR';
measurement = flex.query(':MEASure:EYE:DJ?')
else:
details = flex.query(':MEASure:EYE:DJ:STATus:DETails?')
reason = flex.query(':MEASure:EYE:DJ:STATus:REASon?')
Child commands for measurement identification:
:MEASure:EYE:DJ:SOURce:MEASure:EYE:DJ:RJSValue:EYE:MEASure:EYE:DJ:RJSTabilize
Common Measurement Queries
:COUNt?,:LOCation?,:MAXimum?,:MINimum?,:MEAN?, and:SDEViation?common measurement queries.
Example Command Sequence
:SYSTem:MODE EYE :MEASure:EYE:DJ:SOURce CHAN1A :MEASure:EYE:DJ?