:MEASure:EYE:TJ:TJBer
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:TJ:TJBer
Query Syntax
:MEASure:EYE:TJ:TJBer?
Description
Sets the probablility (BER) for making the Total Jitter (TJ) measurement. The default value is 1 x 10–12 (1E-12), which is a probability of occurrence of less than 1 part per trillion. The query form of the command returns the current probability value.
Requires Option 401, Advanced Eye Analysis Software license.
Requires FlexDCA revision A.02.50 and above.