:MEASure:EYE:JN:EYE

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:JN:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:EYE:JN:EYE?

Description

This command allows you to select an eye on PAM4 signals on which to perform the JN measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. If you experience difficulties measuring a PAM4 signal, confirm that the signal-type setting is set to PAM4 with the :CHANnel:SIGNal:TYPE command.

NRZ Waveform
PAM4 Waveform

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.05.30 and above.