:MEASure:EYE:JN:SJN

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:JN:SJN {J2 | J5 | J9}

Query Syntax

:MEASure:EYE:JN:SJN?

Description

Selects a J2, J5, or J9 measurement results for TJ associated with a specific symbol error ratio (BER).

J2
Associates TJ with a measurement BER of of 2.5 x 10−3.
J5
Associates TJ with a measurement BER of of 2.5 x 6−6.
J9
Associates TJ with a measurement BER of of 2.5 x 10–10.

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.02.50 and above.