:MEASure:EYE:PAM:EHEight:EYE
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:EHEight:EYE EYE{0:6}
Query Syntax
:MEASure:EYE:PAM:EHEight:EYE?
Description
This command allows you to select an eye on PAM4 signals on which to perform the :EHEight measurement. For NRZ signals, the argument EYE0 is automatically selected and cannot be changed. If you experience difficulties measuring a PAM4 signal, confirm that the signal-type setting is set to PAM4 with the :CHANnel:SIGNal:TYPE command.
Requires FlexDCA revision A.04.50 and above.