:MEASure:EYE:PAM:EHEight:DEFine:EOPening:RJSTabilize

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:MEASure:EYE:PAM:EHEight:DEFine:EOPening:RJSTabilize {ON | OFF}

Query Syntax

:MEASure:EYE:PAM:EHEight:DEFine:EOPening:RJSTabilize?

Description

Turns on or off RJ stabilization for PAM4 Eye Height and Eye Width measurements. When RJ stabilization is on, use the :MEASure:EYE:PAM:EHEight:DEFine:EOPening:RJSValue command to enter the RJ value. To determine the RJ, switch the N1000A to Jitter Mode and measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument.

The following lists shows that the stabilization and value settings are linked for PAM4 Eye Heights and Eye Widths measurements. Because the RJSTabilize commands control the same setting, you can use either of the two commands to turn RJ stabilization on or off. Also, because the RJSValue commands enter or query the same variable, you can use either of the two commands to change or query the RJ value.

Linked RJ Stabilization (On / Off) Commands

Linked RJ Value Commands

Requires FlexDCA revision A.05.30 and above.