:MEASure:EYE:PAM:OVERshoot
Command Syntax
:MEASure:EYE:PAM:OVERshoot
Query Syntax
:MEASure:EYE:PAM:OVERshoot?
Moves the PAM4/6/8 Overshoot measurement to the top of the Eye Mode Results measurement results. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. PAM4/6/8 Overshoot is an IEEE 802.3cu compatible measurement.
The PAM Overshoot measurement is reported as a percentage and is defined as:
Where:
- Pmax is based on a 1e-2 hit ratio, where Pmax is the smallest power level that results in the number of samples above that level not exceeding the product of hit ratio and total number of observed samples. All samples are acquired in a single unit interval eye diagram.
The hit ratio's default setting is 1e-2 and is based on the IEEE 802.3cu standard. However, you can change this ratio using the :MEASure:EYE:PAM:OVERshoot:THRatio command.
Requires FlexDCA revision A.06.60 and above.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement,
flex.write(':SOURce CHAN1A')
if flex.query(':STATus?') == 'CORR';
measurement = flex.query('?')
else:
details = flex.query(':STATus:DETails?')
reason = flex.query(':STATus:REASon?')
Common Measurement Queries
:COUNt?,:MAXimum?,:MINimum?,:MEAN?, and:SDEViation?common measurement queries.