:MEASure:EYE:PAM:OVERshoot:THRatio

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

EYE:PAM:OVERshoot:THRatio <hit_ratio>

<hit_ratio> is a double.

Query Syntax

EYE:PAM:OVERshoot:THRatio?

Description

Sets the hit ratio for the PAM4 overshoot measurement (:MEASure:EYE:PAM:OVERshoot. The default hit ratio is 1e-2 which is called out in the IEEE 802.3cu standard. The minimum value is 0.0. The maximum value is 0.1.

Requires FlexDCA revision A.06.60 and above.