:MEASure:EYE:PAM:PMAX:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:PMAX:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:MEASure:EYE:PAM:PMAX:SOURce?
Query Response
<source_waveform>
Description
Selects the source waveform on which to perform the :MEASure:EYE:PAM:PMAX measurement.
Requires FlexDCA revision A.06.60 and above.