:MEASure:EYE:PAM:PMAX:THRatio
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:PMAX:THRatio <ratio>
Query Syntax
:MEASure:EYE:PAM:PMAX:THRatio?
Description
Enters the hit ratio used by the Pk-Pk Amplitude measurements. The default hit ratio is 1e-2 which is called out in the IEEE 802.3cu standard.
Requires FlexDCA revision A.07.60 and above.