:MEASure:EYE:PAM:TPEXcursion:LOCation?
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8
Query Syntax
:MEASure:EYE:PAM:TPEXcursion:LOCation?
Description
Returns an location index of the Transmitter Power Excursion measurement for PAM4 signals in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.
Requires FlexDCA revision A.06.70 and above.