:MEASure:EYE:PAM:UNDershoot:LOCation?

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Query Syntax

:MEASure:EYE:PAM:UNDershoot:LOCation?

Description

Returns an location index of the :MEASure:EYE:PAM:UNDershoot measurement for PAM4 signals in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.

Requires FlexDCA revision A.06.60 and above.