:MEASure:EYE:PEAK
Command Syntax
:MEASure:EYE:PEAK
Query Syntax
:MEASure:EYE:PEAK?
Description
Moves the database Peak Hits measurement to the top of the Results table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. The "Peak" annotation label is displayed which identifies the location of the measurement. The following picture shows the annotation which moves to reflect changes in the location of the peak hits. The database is 521 points high by 751 points wide and is used for histograms, mask testing, and color grade-gray scale displays. Behind each database point is a counter which is incremented each time a pixel is hit by data from a displayed waveform, color-grade memory, or function. Query this command to return the peak value recorded in any of the database counters. The maximum count (saturation) for each counter is unlikely to occur as it is greater than 2 giga-hits. Sources can be any displayed waveform, color-grade memory, or function.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:EYE:PEAK
flex.write(':MEASure:EYE:PEAK:SOURce CHAN1A')
if flex.query(':MEASure:EYE:PEAK:STATus?') == 'CORR';
measurement = flex.query(':MEASure:EYE:PEAK?')
else:
details = flex.query(':MEASure:EYE:PEAK:STATus:DETails?')
reason = flex.query(':MEASure:EYE:PEAK:STATus:REASon?')
Child commands for measurement identification:
:MEASure:EYE:PEAK:SOURce
This Eye mode measurement can be applied to both NRZ and PAM4 waveforms.
Example Command Sequence
:MEASure:CGRade:PEAK:SOURce CHAN1A :MEASure:CGRade:PEAK :MEASure:CGRade:PEAK?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:EYE:PEAK:STATus?')):
measurement = Flex.query(':MEASure:EYE:PEAK?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:EYE:PEAK:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:EYE:PEAK:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:EYE:PEAK?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.