:MEASure:EYE:RJ:SOURce

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:RJ:SOURce <source_waveform>

Where <source_waveform> can be one of the following:

  • CHANnel{1:8}{A|B|C|D}
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:16}

Query Syntax

:MEASure:EYE:RJ:SOURce?

Description

Selects the source waveform on which to perform the RJ measurement.

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.02.50 and above.